Platform
  • RVC
  • Features
  • Depth
  • Deployment
  • Camera Sensors
  • Environmental Specifications
  • Comparisons

OAK-D ProShopDatasheet

Based on
Connection

USB 2/3 (up to 10 Gbps)

Dot projector
Infrared
Yes
IMU
Yes
Sensor 1, 3 - OV9282
Type
Monochrome
DFOV / HFOV / VFOV
Size
1/4
Shutter Type
Global
Focus
Fixed
Sensor 2 - IMX378
Type
Color
DFOV / HFOV / VFOV
Size
1/2.3
Shutter Type
Rolling
Focus
Auto
Stereo
IR Projector

Looking for more details? Visit specific features at Platform -> Features

RVC2 inside

This OAK device is built on top of the RVC2 architecture, with main features being:

Stereo depth perception

This OAK camera has a baseline of 75cm - the distance between the left and the right stereo camera. Minimal and maximal depth perception (MinZ and MaxZ) depends on camera FOV, resolution, and baseline - more information here.
  • Ideal range: ~80cm - 12m
  • MinZ: ~20cm (400P + extended disp), ~40cm (400P OR 800P + extended), ~80cm (800P)
  • Median depth accuracy (See these docs for more info):
    • below 4m: below 2% absolute depth error
    • 4m - 7m: below 4% absolute depth error
    • 7m - 10m: below 6% absolute depth error

IR perception

The Pro version of this device has notch IR filters at 940nm on the stereo camera pair, which allows both visible light and IR light from illumination LED/laser dot projector to be perceived by the camera.

IR Dot Projector

The IR laser dot projector projects many small dots in front of the device, which helps with disparity matching, especially for low-visual-interest surfaces (blank surfaces with little to no texture), such as a wall or floor. The technique that we use is called ASV - conventional Active Stereo Vision - as stereo matching is performed on the device the same way as on OAK-D (passive stereo).On the image below there's a blank wall with no texture. Without the dot projector, (passive) depth perception is poor. With the dot projector set to ~200mA, the (active) depth perception looks much better. If you look closely at the bottom left frame, you can see little dots all around the wall.

IR Illumination LED

Flood IR LED illumination allows perceiving low-light and no-light environments. You can run your AI/CV processes on frames that are illuminated by the IR LED. Note that the color camera doesn't perceive IR light, so you would need to use a mono camera stream for your AI/CV processes.

Getting started

You can set IR laser dot projector and illumination LED via the API as below:
Python
1# Either within Script node:
2script = pipeline.create(dai.node.Script)
3script.setScript("""
4  Device.setIrLaserDotProjectorIntensity(0.5)
5  Device.setIrFloodLightIntensity(0)
6""")
7
8with dai.Device() as device:
9  # Or, using the dai.Device object from the host:
10  device.setIrLaserDotProjectorIntensity(0.5) # in %, from 0 to 1
11  device.setIrFloodLightIntensity(0.0) # in %, from 0 to 1

Dot projector specifications

Ams Belago1.1 Dot-Pattern Infrared IlluminatorDatasheet
Number of dots
4700
HFOI* 50%
78 ± 7%
VFOI* 50%
61° ± 7%
VSCEL wavelength
940nm
Operating temperature
10°C to ~60°C
Temperature absolute limits
0°C to ~80°C
FOI = Field of illumination. Also note that in the datasheet, HFOI and VFOI are switched, that's because we mount the Belago1.1 rotated as we want greater horizontal field to match field of cameras.Regarding operating temperature; some customers use dot projector even at lower ambient temperatures, but first wait a few minutes for device to heat up (by running AI/CV/stereo depth...) so projector gets to above 0°C.

Power consumption

Most of the power is consumed by the RVC2, so the power consumption mostly depends on the workload of the VPU:
  • Base consumption + camera streaming: 2.5W - 3W
  • AI subsystem consumption: Up to 1W
  • Stereo depth pipeline subsystem: Up to 0.5W
  • Video Encoder subsystem: Up to 0.5W
To reduce the power consumption, you can reduce FPS of the whole pipeline - that way, subsystems won't be utilized at 100% and will consume less power. You can also decrease power (and brightness) of the illumination LED and dot projector to reduce the overall power consumption of the device.

Illumination LED and laser dot projector

Power configurable (more power - more brightness):
  • Dot projector (active stereo): Up to 1W
  • Illumination LED (night vision): Up to 1W
Pro devices might consume up to 15W of power, so it's recommended to use external 15+W power supply with Y-adapter.

IMU

This OAK camera has an integrated BNO086, a 9-axis IMU (Inertial Measurement Unit). See IMU node for the API details on how to use it.

Operating temperature

The ambient operating temperature of RVC2-based devices is between -20°C and 50°C when fully utilizing the VPU.Similarly to the power consumption, the max operating temperature depends on VPU utilization. The higher the VPU utilization, the more heat the VPU will generate. The RVC2 VPU can continuously operate at 105 °C, after which the depthai library will automatically shut down the device (to avoid chip damage).To find out more, see our Operating Temperature documentation.

Vibration Testing

This OAK device has been tested for vibration tolerance according to the EN 60068-2-6:2008 standard:
  • Vibration Report - Report of the vibration stress tests performed by the SIQ (3rd-party lab)
  • Vibration Results - Results of Camera Focus, Camera Angles, and Stereo Depth Accuracy before and after the vibration stress tests
More information can be found at Vibration Tolerance documentation.

Similar models

Laser Safety

This product is classified as a Class 1 Laser Product under the EN/IEC 60825-1, Edition 3 (2014) internationally.
  • Do not power on the product if any external damage was observed.
  • Do not attempt to open any portion of this laser product.
  • Invisible laser radiation when opened. Avoid direct exposure to the beam.
  • There are no user serviceable parts with this laser product.
  • Modification or service of the stereo module, specifically the infrared projector, may cause the emissions to exceed Class 1.
  • No magnifying optical elements, such as eye loupes and magnifiers, are allowed.
  • Do not try to update camera firmware that is not officially released for specific camera module and revision.